Part Number: SN65LVDS1
Other Parts Discussed in Thread: SN65MLVD047A,
Hello,
I need to drive 6 LVDS recievers with only one driver in a multidrop topology, at 100MHz clock frequency.
I didn't find a single MLVDS driver ( there is 2 or 3 components with 4 channels or transceivers but no single driver) to realized the function.
My project is driven by saving space and power saving.
One of differences between LVDS driver and MLVDS driver is the output current .
On the MLVDS driver SN65MLVD047A datasheet, the number of nodes is from 2 to 32 with a maximum output current of 24 mA. (FYI, package too large for my design)
In my case, I need only 6 nodes on one very short adapted differential trace, 10 cm maximum between the source and the last recievers at a maximum frequency of 100MHz.
Q1 : Can I use the SN65LVDS1 (output current 10mA) single driver (or equivalents with 2 driver max) to drive 6 recievers with multidrop topology?
Q2 : What is the formula or method to estimate the maximum current need to drive in function of nodes numbers, trace lenght and speed?
Thanks for your support.
Julien.
SN65MLVD047A