Part Number: TPS65983
Dear Sir:
On Thunderbolt Titan Ridge, we are using TPS66983 to develop PD function. and type C PD function only includes 3A@5V, not 6~20V. So I have some questions. Thank you.
1.Please help confirm TPS65983B settings
2.PW_VCCHV_SYS is not supported. What should SENSEP/SENSEN (ball B10, A10) be setted? And HV_GATE1/2 (A9/B9) does not support 6-20V. How to deal with this?
3.SPI ROM,
A. What is the information thant burned in it? Who should I ask to provide it?
B. Intel CRB circuit diagram shows TPS65983B and Titan Ridge are both directly connected to ROM, whether this means that both ICs will read ROM data?
4.When to use ResetZ? When to use MReset? Correspondingly, what will happen if I don't apply these functions?
Thank you very much.