Part Number: SN65LV1224B
Other Parts Discussed in Thread: SN65LV1023A
Hello,
I stuck with deserializers sync lock too.
I have one units where this lock going crazy - up and down. The condition from LVDS didn't changed at all.
But the question is elsewhere :)
Few years ago everything with these deserializers worked very well. But before few month ago something happens to something - some of them are loosing data sync lock.
Our system consist of MT9V032 image sensor, source of LVDS signal, then on signal path lies 2 common mode filters, 100R terminatign resistor and then LVDS receiver - SN65LV1224B.
At the system POR load, we enabling test pattern from MT9V032 to LVDS ine of 0x800 (12bit, start byte 1, rest are zeros) .
Then everything going well and frame are pulled out. And, between the frames, Image sensor sending 0x804.
Can be this some kind of issues to lost sync?
Are need deserializers to re sync frequently?