Part Number: SN65DSI84
Other Parts Discussed in Thread: DSI-TUNER
Hi Team,
There is no display when use SN65DSI84.
The solution is T7'sMIPI(1920x720)->SN65DSI84->LVDS ->DS947->DS948->LCD Display(LVDS).
Verification process:
1. We directly sent the LVDS signal to 947 and the image can be displayed (it was verified that there was no problem with 947/948);
2. We connect the Qualcomm's MIPI signal (1280x720) to the DSI84, and there was a horizontal snowflake dot;
Special note:
We use T7 to do double screen display with two signals
Channel 1: double lvds-> ds947-> ds948-> LCD display (normal display)
Channel 2: MIPI(1920x720)->SN65DSI84 turn dual lvds-> ds947-> ds948-> LCD display (no image display)
Could you please help for this? Thanks a lot!