Part Number: DP83867E
Hello Team, could you help with the below?
One of my designs would like to perform some signal integrity analysis using the DP83867E component. They would like to use the TD_M_C pin to transmit a differential signal which should be possible according to the DP83867 datasheet.
The DP83867E IBIS file only allows the TD_M_C pin to be used as an input.
Is there any way that we could model the TD_M_C pin as an output of a differential pair?
Thanks for your help!