Part Number: DS90UB954-Q1
Dears,
I wander if the i2c controlling information will be blocked somewhere in the following design, anyone could give me some answer?
And will the design work well? Any other potential problems beyond my consideration?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Dears,
I wander if the i2c controlling information will be blocked somewhere in the following design, anyone could give me some answer?
And will the design work well? Any other potential problems beyond my consideration?
Dear Charley Cai,
Thank you very much for the replying.
Yes, you are right. The bypass is to get a replicated video data from the camera sensor for other devices, and those devices would only receive video data without trying to control the camera sensor.
The camera sensor would be controlled by the CPU through the red i2c bus in the figure. The red i2c lines are traces on printed circuit boards.
The CPU here might be replaced by an image processor, and it would regularly write to or read from the remote camera sensor through i2c bus during receiving the image stream. Because the i2c transactions will pass across 2 954-953 chains, and I want the video to be 30 frames per second, should the i2c timing be a problem here?
Best regards,
Tang Yaosheng