This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: How to enlarge the max speed of csi input of UB953?

Part Number: DS90UB953-Q1

Dear Sir,

According to UB953 spec, the max speed of csi input is 26Mhz*128/4 = 832Mbps(800Mbps for 25Mhz), but some image sensor will output about 1Gbps per lane even its effective payload doesn't need this such high speed.

So, How to make UB953 to receive higher speed mipi clock, for examples, 1Gbps for single lane?

Best,