Part Number: DP83867IS
Hello All,
I have a question about the RGMII bus on the DP83867 PHY.
In my application, I have 2 DP83867 PHYs that have the RGMII-Rx tied to RGMII-Tx of the other PHY. This set up is working as expected. I have 2 questions:
1) When I look at the signal levels on the RGMII bus, the RX clock has a signal swing of about 1v p-p and the data lines are about 200mv p-p. Both of these seem on the low side to me. What voltage rail is associated with the RGMII interface, and is there any reason these signals are not higher??
2) When I set my test equipment to run random side packets (64 byte to 1514 byte), I get CRC error-ed packets. If I set my packet sizes to transmit a single size packet, I run no errors. (I have run streams with only 64 byte packets and streams with 9000 byte packets - no errors)
Wondering if anyone has thoughts on this,
Thanks,
Mike