Part Number: TUSB8020B
I have the same troubble as Petr Zkrat reported 6 months ago.
Is there a solution for it?
BR
Fredrik Karlemon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8020B
I have the same troubble as Petr Zkrat reported 6 months ago.
Is there a solution for it?
BR
Fredrik Karlemon
Yes
Booth options with board powered by VBUS and Hub powered by target is tested.
The circuit get the chrystal oscillating in booth configutations for 60% of the boards.
1. I have got one out of 5 failing boards to work after dismount/remount the same circuit.
Bad connection for the ground-tab isn't the only problem with the circuit.
2. Variation of resistive (680k, 820k, 1M, 2.2M, None) and captive (5.6p, 12p 18p, 22p) load to the chrystal
(CTS 445C25D24M00000, 24MHz ±20ppm Crystal 18pF 40 Ohms) gives no result to the port.
3. Variation of the reset delay (2ms, 10ms, manual) gives no difference.
Is there any other IO's involved in the internal oscillating circuitry than 3V3, GND, GRST, XI and XO?
You asked about USB_VBUS-pin and if HOST is connected - does that really make any difference in this case?