Part Number: DP83640
Hi team,
The customer is testing with two DP83640-EVMs to achieve IEEE1588 operation. They are referring to software development guide but cannot achieve 1PPS output from GPIO9 in condition of the below connection. The EVM setup is done by Win10 PC via MSP430 Launch Pad (USB to MDIO).
GPS -> EVM-1 -> Ethernet cable -> EVM-2
The customer could change CLK_OUT to 10MHz from 25MHz but they cannot output 1PPS from EVM-1 and EVM-2, respectively.
(1) Could you please provide the register dump of all the settings for both SNLA098A and SNOA548A? They would like to check what their setting is wrong by comparing with the settings of app notes.
(2) As above connections, they don't use MAC layer for the 1PPS transmission in this testing. Do you think the MAC is needed for the 1PPS output from DP83640?
Regards,
Jun