Part Number: TUSB8041
Team,
my customer is using TUSB8041 in a new design. The device is directly connected to a CPU with its upstream ports. There is no connector etc.
Only the data signals are connected, there is no switchable upstream VBUS voltage. The USB_VBUS pin of the hub is directly connected to the 5V supply on the board.
Is this setup USB compliant?
How do they need to handle USB_VBUS to be USB compliant?
The TI EVM uses a VBUS switch between hub and CPU. Is this needed?
Is the connector that is used on the EVM also needed?
What's the recommended circuitry for the hub if it is directly connected to the upstream port without having a complete USB-host with VBUS?
Thanks!