Part Number: TPS65987D
Other Parts Discussed in Thread: TPS6598X-CONFIG
Hi Team,
My Customer is going to evaluate the TPS65987D with SPI-Flash Less System. Their external hosts (SoC) does download the patch bundles (containing the application configuration and code patch) to the SRAM of the TPS65987D over I2C.
They refer Application Report "TPS65987DDH Host Programming for SPI-Flash Less Systems". There is example code in the Application Report, but it is not easy to understand them. If there is the Patch Bundles example for the following operation, could you let me show that?
***********************************************************************************************
Boot Mode Pin Strapping: ADCIN1 DIV = 0.30 ~ 0.38
<Dead Battery Mode> BP_ECWait_Internal
The internal power switch from VBUSx to PP_HVx is enabled for the port receiving power. The device infinitely tries to load configuration.
&
<Device Configuration> Infinite Wait
Device infinitely waits in boot state for configuration information.
***********************************************************************************************
TPS65987D is set as follows first,
- Power Role: DFP, PDO=5V/3A
- Data Role: DFP
TPS65987D waits connection of device
After connection of device was done, if it is possible to swap the Data Role,
- Power Role: DFP
- Data Role: UFP
***********************************************************************************************
Thank you.
Best Regards,
Koshi Ninomiya