Part Number: TUSB9261-Q1
If the terminal status differs depending on the FW version, or if there is an update for Fig16, please tell me the terminal status again.
(Supplement)
Currently, the FW used is Ver.1.06.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261-Q1
If the terminal status differs depending on the FW version, or if there is an update for Fig16, please tell me the terminal status again.
(Supplement)
Currently, the FW used is Ver.1.06.
GPIO for firmware v1.06 is described on Table 1 in section 7.3.1.3 of the TUSB9261 datasheet.
Regards,
Please tell me the pin state (input / output and logic) immediately after reset release during device reset in FW: v1.06.
It is the same as what is described in Table 1 in section 7.3.1.3 of the TUSB9261 datasheet. You can find it on page 12. Is there something missing from the table that you would like to know?
================================================================
I/O | LED | Usage
================================================================
GPIO0: - [INPUT with 100uA PD] Undefined. Can use HID commands to change to output low or high.
GPIO1: - USB 3.0 Link State if U1/U2 enabled, otherwise [INPUT with 100uA PD].
GPIO5: - USB 3.0 Link State if U1/U2 enabled, otherwise [INPUT with 100uA PD].
-----------------------------------
State: GPIO1/GPIO5 state.
-----------------------------------
U0: Off/Off.
U1: On/Off.
U2: Off/On.
U3: On/On.
Other: Off/Off.
GPIO3: - [INPUT with 100uA PD] Momentary Push Button (for remote wake).
GPIO4: - [INPUT with 100uA PD] Bus or Self-powered Indicator. (GPIO level should be HIGH when self-powered)
GPIO6: - [INPUT with 100uA PD] Undefined. Can use HID commands to change to output low or high.
GPIO7: - SS Connection.
GPIO10: - [INPUT with 100uA PU] Undefined. Can use HID commands to change to output low or high.
GPIO11: - [INPUT with 100uA PU] Power Fault Indicator.
PWM0: - Disk Activity (LED blink rate is faster when connected at USB SuperSpeed), USB connection (LED On), and USB Suspend (fading LED).
PWM1: - SW Heartbeat.
Regards,