Part Number: TUSB3410
Tool/software: Linux
Hi,
is the device detected as I2C Controller or as some virtual COM Port or how can i communicate with it under Linux when it is used as USB to I2C bridge?
We need to communicate with a custom Front Panel that has an I2C bus interface. It is connected to a PC / Server Board and the internal I2C Busses are not accessible. So we thought this USB to I2C bridge could be used to add another I2C interface / controller. Ideally the linux i2c-tools can be directly used (i.e. i2cdetect, i2cget, ...).
Best Regards,
Sebastian