Part Number: TLK2711-SP
Hello
In my card the TLK2711A is connected to a Virtex4 FPGA.
To consume power at standby mode we turn off the TLK2711 Vdd and deactivate the FPGA by pulling down its ProgB pin (its HSWAPEN pin is at "0").
Point is that in such situation the FPGA deliver "1" over its all IO pins, thus the SerDes IO pins fills 2.5V where its Vcc=0.
This is an obvious violation of the "Absolute Max Rating" demanding that Vih < Vdd + 0.3
However, the FPGA "1" while at ProgB state (NOT loaded) is actually delivered by its internal very weak pull up (200uA max at Vdd=2.5V)
Is such a low current can harm the powered off SerDes?
Can I disregard the above violation?
Can I continue with the above power down saving scenario?
Looking forward to hear from you.
Thanks
Amnon