Part Number: SN75LVCP600
Other Parts Discussed in Thread: DS125BR111, , DS80PCI102
Hi there:
Our customer would like to check an question about the description is the spec, could you help us to reply that?
- Multirate operation for 1.5G, 3G and 6G and specification also support PCI Express 3.0 ( 8G ).
Can you help to check the Multirate support 8Gbps or not?
2. As we know the PCI Express 3.0 ( 8G speed ) energy in the 4GHz.
But specification just show in the 3GHz.
We want to know the performance in the PCI Express 3.0