Part Number: TUSB8020B
hi
I am developing a usb hub.
I want to connect the phone to type c, charge the current through the type A connector on the usb hub, connect the mouse and use the screen of the phone
The current is charging and the connection with the mouse is not working.
I have three requests.
I want you to take a look at my circuit.7587.qusetion of tusb 8020b curcuit-페이지-4,12.pdf
Also, I would like to ask if I can input 3.3V input to SMBUSz / SS_DN2 to enter I2C mode of TUSB8020b
Finally, I'll ask for a utility that can create an EEPROM. Please answer Thanks