Other Parts Discussed in Thread: ALP, DP83867E, LMH0397, LMH0324
I am using the LMH0387 Line Drivers on the SD387EVK dev board kit and trying to test the extended 3G reach mode to see the max length we can push SGMII and Ethernet signals over RG179 (75 ohm Coax cable). We are pairing the SD387EVK dev board with the DP83867E-SGMII-EVM dev board to push Ethernet over our coax lines.
The RG179 cable has a lot worse loss than the Belden 1694A cable specified on the LMH0387 datasheet. We are using the RG179 cable instead of the Belden 1694A cable because there are spare RG179 cables that we are looking at using on our existing platform of interest. FYI the RG179 cable we are using is specified to have attenuation of 21 dB/100 ft at 400 MHz.
When we turn on Extended 3G Reach Mode either by using the Analog LaunchPAD (ALP) software or by writing to the SPI Register Address 00h bit 2, we are unable to increase our max length.