Part Number: DS90CR288A
Hello
In application note SNLA249, figure 4, TX data toggle at internal Rx clock falling edge then strobe it at internal RX clock rising edge.
If no skew between RxCLKIN and RxIN, Tx send data and clock as the same manner as Figuire 4. Is my understanding correct?
I think the period of setup and hold time of Ideal Rx Strobe position(C area of datasheet figure 16) is below. Is my understanding correct?
C period = [The biggest number of Rsposn min( = the longest number of each bit setup time)] - [The biggest of Rsposn min (= the longest number of each bit hold time)]
We try to calculate the worstest marign of RSKM. I think worst case is Rsposn_max - Tpposn_max but application note used Rsposn_min. Do we misundersatand something?
Best regards,
Toshihiro Watanabe