Part Number: TPS65982
The product is Docking, inside docking is 982 device, 982 act as sink, and NB act as source, 5V voltage. I set FW below configuration,
1. OVP trip point: 24V
2. High voltage warning level : Warning when source VBUS voltage exceeds 20% ....
3. Low voltage warning level, Warning when source VBUS voltage dips below 20% ....
Now we find NB sourcing 982, VBUS voltage will high to 6.5V, then CC disconnection.
So we highly suspect the error is coming from NB , and not sure when 982 is sink, how about the OVP point when 5V? 24V? or 5*( 1+20%) = 6v?
When high voltage warning level comes t0 6V, VBUS will be disconnected.
Please support here, Thanks,