Part Number: DS90UB960-Q1
Hello,
In continuation with my previous question asked in the forum, I have designed a 100ohm differential trace on a PCB instead of coax cable for FPD-Link III communication between UB953 and UB960. However, I am having some issues with forward communication between UB953 and UB960 (CSI-2 Data packets not received correctly). I was able to communicate successfully with UB953 using back-channel frequency of 50 and 25Mhz. I read the following registers in UB960 for verification
Register 0x4D: Value=0x13
Register 0x4E: Value=0x4d
Register 0x7A: Value=0x0f
From the register values, it seems that I am having the CSI-2 data packet error. The major difference in my hardware is that I have currently designed my differential trace as shown in Figure 44 for STP Connection, Page 153 of UB960 datasheet instead of Figure 45 single ended coaxial, Page 153 in the same datasheet. Both single ended and differential trace configuration should ideally work. In UB964 Datasheet, Register 0x6D[2] (Page 79) can be used to do this setting where we can choose between coax and STP mode. However, I did not find anything similar in UB960 datasheet. Is there any register to select the correct mode for FPD-Link III communication between coax and STP?
I look forward to your reply. Thank you.
Best Regards,
Nishant