Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
HI TI guys
- The DP83869 evm runs in 1000M media converter, but one of stranger thing is the copper interface always be running in 100Mbps.
The register is setting on the below
x01DF -> 0044
x01EC -> 1FFC
x0000 -> 1140
x0010 -> 5048
x0C00 -> 1140
Do you have any suggestion?
2 SFP module in plugged in the SFP cage and make sure the module is OK.
The FX_VCC is external power, normally the SFP module power consumption is 170mA @3v3, but in this case the SFP power consumption is only about 120mA @3v3, also it is no optical power output.
Can you please let me know the situation?