This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP119: Display eDP Content on DP Monitor

Part Number: SN75DP119

Hi Team,

I am planning to propose a solution to test the eDP interface on my board using a standard monitor that supports DP.

1. Do we need any bridge IC to convert eDP to DP?

2. Can I route the eDP main link signals(Lane 0 & Lane 1) from SN75DP119 directly to standard DP connector? 

3. How can I terminate the unused pins of standard DP connector(Lane 2 & Lane 4)?

--

Thanks & Regards

Gireesh

  • 1. no, you don't need bridge IC to convert eDP to DP

    2. sure, you can

    3. you don't need to terminate un-used channels. DP itself can be one lane two lane and four lane