Part Number: DS90CF386
Dear Support Center,
There are four additional questions.
Q1) If the clock frequency is not 85 MHz, will the jitter range be the same as 85 MHz?
For example, 25MHz, 54MHz, 65MHz.
Q2) Does DS90CF386 support Spread Spectrum Clocking?
Q3) If Spread Spectrum Clocking is enabled, do we need to comply with the jitter standard (150 ps)?
Q4) There are two statements in the datasheet about Jitter, which one should we judge?
[6.6 Switching Characteristics] : clock jitter (less than 150 ps).
[Figure 13. Receiver LVDS Input Skew Margin] : Cycle-to-cycle jitter depends on the Tx source. Clock jitter should be maintained to less than 250 ps at 85 MHz