This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer asked for a solution to transmit data with high speed, below is the SPEC, Would you please a suitable solution? thanks.
1. bi-directional
2. 3m distance.
3.about 200M bps data rate.
4.easy to interface with FPGA.
Hello Yue,
MLVDS is a good option for this application. Do they need 4 channels? If so, then DS91M040 is an option. If they only need 1 channel, then SN65MLVD206 is a good option. How many devices will be on the bus, is it just the 2 FPGAs? If that's the case, then they should be able to achieve 200Mbps rate at 3m distance, but it may depend on the cable - CAT5 or similar should be fine. The above 2 devices are half-duplex (sharing the same differential pair for transmit and receive). We have devices that are full duplex (e. g. SN65MLVD207), which will require a pair for each direction.
Regards,
Yaser