This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: Max FPDL3 resolution 720p?

Part Number: DS90UB947-Q1

I want to confirm the maximum resolution that one FPDL3 link is able to transmit? It's 720p?
This will confirm my suspicion about the reason DS90UB947-Q1 use two FPDL3 (dual link) to transmit 1080p.
Regards,

  • Your suspicion is correct. 947 need dual link to transmit 1080p.

    We care more about actual video data rate. A single link can support about 2.3Gbps of actual video data. The actual resolution is a little higher than 720p, but cannot support 1080p with a single link.

    Best Regards,

    Charley Cai