Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869EVM
Hi E2E,
Good day!
May I now what would be the correct voltage level for the VDD1P1 connection? As indicated on the Pin Function table, these pins are for 1.1-V Analog Supply and on the design requirement these should be connected to 1.1V supply. However, on figure 116, these pins are supplied by 1.0V. and named as VDD1P0. This is also the case for the DP83869EVM schematic, http://www.ti.com/lit/df/snlr042/snlr042.pdf. These pins are supplied by 1.0V and named as VDD1P0.
Also, is the current consumption for each voltage rails at different modes available?
Looking forward to your response.
Best regards,
Franz