Part Number: TUSB3410
hi ,
I use the TUSB3410 to transfer UART & USB console .
The schematic is as following.
When I plug in a USB console device to TUSB3410 , the computer display " USB Device Not Recognized" .
So I measured the voltage level :
VCC#3 : 3.3V
VDD18 : ~0.9V
I think VDD18 voltage level is abnormal . and then I check the value of R1266 and R1262.
R1266 and R1262 resistor value is correct , as the schematic appear.
Why is the VDD18 voltage only 0.9V ? Is the TUSB3410 damaged?
Besides.. I did an experiment to prove whether the TUSB3410 is good or damage.
I remove the R1266 and R1262 and R1269 , and then pull down with VREGEN pin.
at this time, measured VDD18 again. After reworking , the VDD18 voltage level is about 1.78V.
But I still can't get the USB device....