Hi,
I am working with the DP83869HM and I have two questions:
1. Could you provide detailed power consumption information (current for each power net) for RGMII to Copper (100M) [100% Utilization] and [50% Utilization].
2. In Hung Nguyen92's reply to Mitchell he references a VDD1P0 power net (Mar 29, 2019). This is not referenced in the schematic which instead references a VDD1P1 power net on page 11 of 'DP83869HM High Immunity 10/100/1000 Ethernet Physical Layer Transceiver With Copper and Fiber Interface datasheet (Rev. A)'. Which is the correct power net?
Thank You!
Alex Montes McNeil