Part Number: TPS65988
Hello Eric,
I would like to confirm which profile was established as a result of negotiation.
I want to use SRDY to turn on the switch if the result is met with the intended profile.
And I want to supply power to the device in the latter stage. Which status register should I check to do this?
Specifically, I want to confirm that the source side has a 1.5A supply capacity.
For example, even though a manufacturer's product specification requires typeC to TypeC,
I am thinking of a situation where the user uses a typeA to typeC cable. At this time,
if only 500mA can be supplied, I would like to create a mechanism that prevents the latter system from starting up.
Best regards,
DDdoor