Part Number: DP83867IR
Hi,
I have used DP83867IRRGZ in my board with MAC which is soft IP in FPGA.
I want the chip works in RGMII mode,so I configure the register with MDIO , but it didn‘t work fine.
The configuration flow is below:
(1) Global reset: Set the bit 15 of register 0x001F to '1';
(2) Advertisment the PHY the 1G mode;
(3) LED register configure;
(4)Strap bit clear: clear the the bit7 of register 0x0031;
(5)Enable auto-negotiation: Set the bit 12 of register 0x0000 to '1';
(6) Set PHY to RGMII mode:Set the bit 7 of register 0x0032 to '1';
(7)Set Clock delay with the register 0x0086;
(8) Restart auto-negotiation:Set the bit 9 of register 0x0000 to '1';
(9)Wait the auto-negotiation complete.
Is the configuration flow correct?
Thanks!