Part Number: TPS65983B
Other Parts Discussed in Thread: TPS65982, TPS65987D
Hi Ti team,
1, Our product is a mobile phone, and we need to use TYPEC interface to record the program of i.m. X8M system. At this time, we need tps65983B, which is to directly connect C_USB_TP, C_USB_TN, or C_USB_BP, C_USB_BN through to USB_RP_N,USB_RP_P.
When the system is not running and I2C cannot configure TPS65983B and the SPI FLASH configured by TPS65983B is empty
2, Please help us confirm whether TPS65983B can realize USB pass-through by default or what are the methods?
3, If TPS65893B cannot be implemented, is there any other IC that can support this function?
4, What are the differences between these IC's TPS65983B,TPS65982,TPS65987D?
5, Is there any configuration software or original code to configure SPI FLASH for TPS6598X for reference?
thanks!