This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: DS90UB947 and DS90UB948 Single Open-LDI configuration

Part Number: DS90UB948-Q1

Hi everyone ,

Can you confirm the following questions of DS90UB947 and DS90UB948 ?

LCD :  800 x 480,  26.2MHz

Single Open-LDI (D0,1,2,3,CLK) -> DS90UB947-> Signle FPD-LINK III -> DS90UB948 ->Single Open-LDI (D0,1,2,3,CLK) 

1.   For unused pins  of DS90UB947 (D4,D5,D6,D7,DOUT1) and DS90UB948 (D4,D5,D6,D7,CLK2, RIN1)  floating 

2.   MODE_SEL0   configured " 010 "   , MODE_SEL1   configured " 000 "  

 -. Is the configuration correct ?

 - .Also need to configure any other  register ?

Thanks,