This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK1101E: Validate LOSL, LOSR, VTH implementation is correctly implemented and understood

Part Number: TLK1101E

Hi,

I am planning on controlling the LOS pins by using SCL/SDA as the control mode and I will be connecting these SCL/SDA pins to an FPGA with pullup resistors.

 For the other pins, I am planning on doing the following even though I will be using SCL/SDA as the control mode:

  • LOSL = open, to have it default on powerup to the lower LOS assert threshold voltage even though I plan on setting register address 0 bit 0 for the serial control mode
  • LOSR = connecting to FPGA to be configured
  • VTH = open, for default 0V differential threshold.

Let me know if you see any problems with this approach or if this is correct.  

Thanks,

HSG