Part Number: TUSB320EVM
Other Parts Discussed in Thread: TUSB320
In a new product design, I have a USB Full Speed peripheral on custom hardware, which will connect to a cell phone with a USB-C port.
It must operate in one of two modes.
Mode 1: Phone is host. Peripheral is connected. Peripheral supplies its own power. Or, ideally, the phone is a host and is also receiving a charge.
Mode 2: Phone is disconnected from peripheral. Phone is receiving a charge.
Can the TUSB320 chip change modes on the CC lines to accomplish this?
If not, is there some other chip that can accomplish this?
Am I better off just putting in circuitry to enable pull-up and pull-down resistors on the CC lines?