Part Number: TPD3S714-Q1
Hi Sir,
I have some questions about power consumption and behavior need your help to clarify it.
Could you please help on below questions?
- When system is in sleep mode(turn off VIN 3P3 supply), will find there is a current draw from VBUS_CONN.
1. Can EN_N disable VBUS_CON to reduce power consumption ?
2. Is EN_N function workable when VIN 3P3 off ?
3. The system doesn’t need 5V from external and we only need VDP/VDN ESD protection function.
Can we just leave VBUS_CON/VBUS_SYS/FLT_N pin as floating?