This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI83: Use SN65DSI83 to display a white screen

Part Number: SN65DSI83

Hi

I used SN65DSI83 to design the screen,but there was a bit of a problem and occasionally the screen was a bit of a blur

1:Increase the output voltage of MIPI to LVDS IC (SN65DSI83ZQER) to verify,it happens about once every 100;It happens about 1/400 times before Increase the output voltage

2:The output voltage of MIPI to LVDS IC (SN65DSI83ZQER) was adjusted back, even it was lower than the original default value. The verification also showed that the white screen appeared for more than 1/100 times, one appeared after more than 1/10 times, and the other appeared after more than 1/400 times. At this time, it was reflected that the LVDS signal was gone

3.Previously, LVDS signals were present even though the screen was flowered,Here is the schematic