Part Number: DP83825EVM
Other Parts Discussed in Thread: DP83825I
Hi Expert,
My customer is using DP83825i now and set DP83825i in slave mode, which is set through the pin 17. They have two questions about the configuration.
1. Without extra configuration, the pin 2 is default to LED0 function. Is it correct?
2. The 50MHz reference clock is used on this application, which registers need to be configured?
They know the RMII_Clock_Selection in RSCR_Register need set to 1 and RMII_Clock_Selection in CR2 register is set to 0(default). Is there any other register need to be configured?