This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3USBA225: when the pin is in OFF mode will the chip drive any logic or will it keep those “OFF” pins in Hi-Z

Part Number: TS3USBA225

One more question on the part.
I see that the part will be in low power mode when SEL1 and SEL2 pins are 0 and similarly one will be active according to the selection.
While that time when the pin is in OFF mode will the chip drive any logic or will it keep those “OFF” pins in Hi-Z? I want to ensure that the pins in OFF during Power-Down mode or during a particular selection would not impact the functionality of pins which are not being used?