This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Q FOR TUSB2077A

1,Can I not use 7 8 47 pin EEPROM? What is the main information stored inside?

2, MODE is low:the APLL output clock is selected as the clock source to drive the internal core of the chip and 6-MHz crystal or oscillator can used

    MODE is high:XTAL1/CLK48 is selected as the clock source and 48-MHz oscillator

What are the purposes of these two modes?
3,What are the purposes of the red circle circuit