This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I: "Functionally there is no need to configure or terminate an unused or non-removable port, but it is required for USB spec compliance. Using OTP a port can be configured as non-removable, but configuring the hub with unused ports requires I2

Part Number: TUSB4041I


RE: "Functionally there is no need to configure or terminate an unused or non-removable port, but it is required for USB spec compliance. Using OTP a port can be configured as non-removable, but configuring the hub with unused ports requires I2C or SMBUS."

So... what is needed to terminate an unused non-removable USB output outside of the USB spec if OTP, I2C, SMBus are not used? 

  • Sorry, my initial response was not clear.  There is never any need to physically terminate an unused or non-removable port.  The USB specification does require a hub to report a non-removable port or an unused port, but functionally the hub does not operate differently based on these configurations.

    Regards,

    JMMN