Part Number: TMDS171
David-san, JMMN-san,
The customer has related questions from the following E2E.
https://e2e.ti.com/support/interface/f/138/t/836082
Now, the customer use default setting of both registers (0Bh, bit 02, 100ksps, 09h bit(1:0) 100ksps), now.
Q1) In above setting, can we use 400kHz signal from HDMI Tx? If not, what happn?
Q2) Should we set both (0Bh bit2 and 09h bit(1:0) ) registers when 400kHz signal is used?
Your advise would be so appreciated.
Best Regards,
Akihisa Tamazaki