Part Number: MAX3221E
Other Parts Discussed in Thread: TRS3122E, TRS3253E,
Dear,Sir
I am working on a project where we have implemented the MAX3221ECPWR IC ,In our application we are communicating with the LCD Interface which Has the same Type of the IC built in it.
But before communicating with the IC implemented in the LCD ,We are doing a manual testing for detection purpose.
My query is mentioned Below:
1)I am unable to detect the IC.We are operating the IC on the 3.3V of supply.
I have disabled the auto shutdown function and connected the force pins with the 3.3 V as displayed in the attached Image.
2)I am unable to generate the Voltage on the 2-4 And 5-6 Pins.
Voltage on 5-6 pins is 1.12V and on 2-4 pins is 0.78v.
What should be the voltage across the 2-4 and 5-6 Pins.?
3)I have connected the usb to UART Dongle and providing the input on the 9-11 Pin ,Still shorting the 8-13 Pin to see whether we are receiving the transmitted data displayed on the dock light.
Still we are unable to receive the transmitted data...!!
Please have a look on the below attached image of the schematic.
Please help on this query your help would be highly appreciated...!!