Part Number: MAX3221E
Hi TI Team,
I'm having a few issues using the TI MAX3221E.
I checked the charge pump and all pins are the same as the datasheet.
V+ : 5.6V and V- : -6.1V
However, RIN (pin 8) drops from -5V to -13V at power-on, receives a data swing below 0V and does not output to Rout (pin 9).
Do you have any idea?
By the way, we implemented the exact same circuit on another board and that board works fine.
Thanks