This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP159: SMARC module and DDC signals

Part Number: SN65DP159


Hello,

Could you confirm if when SDA/SCL from the source is connected directly to the SDA/SCL sink then SCL_SRC and SDA_SRC pins must be pulled to ground or to VCC?

In addition I would ask if SDA_SNK and SCL_SNK can work properly at 3.3Vdc (level shifter with pull up to 3.3Vdc instead of 5V)

Thanks

Lorenzo

  • Lorenzo

    SCL_SRC and SDA_SRC need to be pulled to GND. We have seen cases where noise in the system on the unconnected pins has been interrupted as signaling by the DP159 and has resulted in the DP159 holding the I2C bus indefinitely.

    SDA_SNK and SCL_SNK can work at 5V, not 3.3V.

    Thanks

    David