This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS91M040: Will there be any issue with the device if input signal exists but no power supply for certain duration?

Part Number: DS91M040

Hi,

One of our customer is using MLVDS buffer DS91M040 for backplane clock applications (ATCA compatible). Now when line card having DS91 is not powered then will there be any issue even if backplane clock is coming to this IC while it is not powered up? Will the internal ESD diodes will be creating any issues if the Input Signal is available but not the Power supply to this device? Please clarify.

 

Purna.