Part Number: TUSB7320
Two questions about TUSB7320:
- Does the global reset pin reset the PCIe bus (requiring renumeration)?
- Is the global reset pin an output during startup? Or does it always act as an input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Below is feedback we previously received; please confirm it's accurate?
1)The /GRST terminal of the TUSB7320 is a I/O cell, so it has to be configured as an input or as an output, using a I/O cell for this terminal is a design decision, the host performs this configuration automatically.
It is important to hold the /GRST asserted until all power rails are stable to let the device perform this configuration.
2) The device can’t work without a Global Reset signal at power-up.