Part Number: DP83848-EP
Hi,
Why are we seeing the RX_ER pin go active on us when initiating an FTP file transfer to our :
1. The DP83848 BIST external loopback test passed with flying colors, and,
2.Two identical products successfully perform the file transfer task, i.e, ethernet packets are the same
The MAC FPGA is on the 'other side' of the PHY and should not be a factor as to why the RX_ER pin of the PHY goes high
Thanks