Part Number: TUSB213
Other Parts Discussed in Thread: TUSB217
Hi Sir/Mam,
I would like to share with you that i am using TUSB213 as redriver for extending the usb cable length. Currently i have made my own cable where i have 5m prechannel cable then TUSB213 and then 5 m post channel cable support using the TUSB213 IC. The configuration which i have kept is AC boost is at level 3 and the DC boost is at the highest level.
During testing i have observed that when i connect smaller pendrives/USB to TTL converter the cable works fine. Infact i have tested the cable by reading and writing more than 100gb of data sequentially as well as parallely between the pendrive and the PC using USB 3.0 port and USB 2.0 port as well. I get an average read and write speed of about 25MBps depending on the file size.
When i connect a SSD hard drives the cable detects the SSD and also i am able to send the data to it but at a very slower rate, whereas when i connect 1tb HDDs at the end of the 10m cable then unfortunately the cable fails. At time it detect HDD but doesn't communicate or at times it doesnt detect the HDD at all. I have checked the circuitry and i personally believe that it may be the I2R losses of the cable which may causing the HDD a lower voltage or lesser current due to which the HDD may not be getting sufficient power.
Please let me know if there is any solution for this issue. If there is any IC which i can use along with the TUSB213 to resolve this issue. Thanks
Regards
Piyush