This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD888: what is the maximum current in Differential A and B in RS485

Part Number: SN65HVD888


what is the  maximum current in Differential A and B in RS485 as it is not mentioned in the datasheet.

Please intimate the same.

  • Shivangi,

    Please refer to the Io spec in section 6.4 (page 4) for the maximum current load of each pin. The figure 15 on page 13 shows the equivalent driver schematic. Basically each pair of P/N works independently. The current from one P side flows back to ground through the other N side. I hope this answers your question. If you have concerns about the specific application. Please let me know.

    Regards,

    Hao